I purchased a set of MPC5554 development kit, using the codewarrior2.1 version of the IDE, the suite comes with MULTILINK Rev. C debugger can be normal debugging. But I also bought the MULTILINK Rev. D debugger debugging process error, see the picture. Ho

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I purchased a set of MPC5554 development kit, using the codewarrior2.1 version of the IDE, the suite comes with MULTILINK Rev. C debugger can be normal debugging. But I also bought the MULTILINK Rev. D debugger debugging process error, see the picture. Ho

1,351 Views
huafang
Contributor II
1 Reply

1,254 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

this is rather question to PEMicro support. Could you please try to contact them directly?

PEmicro - P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Develop... 

Regards,

Martin