I have a problem in the installacion de codewarrior 10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I have a problem in the installacion de codewarrior 10.6

747 Views
jorgedaniel
Contributor I

Hi, I have a problem in the installation of codewarrior  10.6, you can not install a driver and I get error code 0x80000000 . finishes installing

but processor expert  not working properly. I install it in an environment of win 8.1 in a notebook .

What could be the problem ?

from already thank you very much

Labels (1)
0 Kudos
Reply
1 Reply

665 Views
TICS_Fiona
NXP Employee
NXP Employee

If Eclipse CodeWarrior usage on Windows Vista, Windows 7 or Windows 8, Administrator rights are required to install CodeWarrior, since the installer copies files into the System folder.

Your project workspace needs to be setup in any folder that you can fully access.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply