I have a problem in the installacion de codewarrior 10.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I have a problem in the installacion de codewarrior 10.6

1,095 次查看
jorgedaniel
Contributor I

Hi, I have a problem in the installation of codewarrior  10.6, you can not install a driver and I get error code 0x80000000 . finishes installing

but processor expert  not working properly. I install it in an environment of win 8.1 in a notebook .

What could be the problem ?

from already thank you very much

标签 (1)
0 项奖励
回复
1 回复

1,013 次查看
TICS_Fiona
NXP Employee
NXP Employee

If Eclipse CodeWarrior usage on Windows Vista, Windows 7 or Windows 8, Administrator rights are required to install CodeWarrior, since the installer copies files into the System folder.

Your project workspace needs to be setup in any folder that you can fully access.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复