I have a problem in the installacion de codewarrior 10.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have a problem in the installacion de codewarrior 10.6

720件の閲覧回数
jorgedaniel
Contributor I

Hi, I have a problem in the installation of codewarrior  10.6, you can not install a driver and I get error code 0x80000000 . finishes installing

but processor expert  not working properly. I install it in an environment of win 8.1 in a notebook .

What could be the problem ?

from already thank you very much

ラベル(1)
0 件の賞賛
返信
1 返信

638件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

If Eclipse CodeWarrior usage on Windows Vista, Windows 7 or Windows 8, Administrator rights are required to install CodeWarrior, since the installer copies files into the System folder.

Your project workspace needs to be setup in any folder that you can fully access.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信