I cannot create a bareboard application with my new install of CodeWarrior 11.1.1 for ARM on my Ubuntu Linux system.  The IDE starts, and I'm able to complete the Create new project dialog.  I click Finish and the dialog stays there, and nothing is create

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I cannot create a bareboard application with my new install of CodeWarrior 11.1.1 for ARM on my Ubuntu Linux system.  The IDE starts, and I'm able to complete the Create new project dialog.  I click Finish and the dialog stays there, and nothing is create

跳至解决方案
1,995 次查看
williamwatts
Contributor II

I cannot create a bareboard application with my new install of CodeWarrior 11.1.1 for ARM on my Ubuntu Linux system.  The IDE starts, and I'm able to complete the Create new project dialog.  I click Finish and the dialog stays there, and nothing is created.

标签 (1)
1 解答
1,860 次查看
williamwatts
Contributor II

I fixed the problem by uninstalling and reinstalling CodeWarrior.  This was for a LS1043 MCU, making an ARMv8 bareboard application.

在原帖中查看解决方案

3 回复数
1,861 次查看
williamwatts
Contributor II

I fixed the problem by uninstalling and reinstalling CodeWarrior.  This was for a LS1043 MCU, making an ARMv8 bareboard application.

1,861 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi william,

Thanks for your response, is good to hear the problem was fixed after reinstalling CodeWarrior.


Best Regards!
Carlos Mendoza
Technical Support Engineer

1,861 次查看
Carlos_Mendoza
NXP Employee
NXP Employee


Hi William,

Could you tell us which MCU are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer