I cannot create a bareboard application with my new install of CodeWarrior 11.1.1 for ARM on my Ubuntu Linux system.  The IDE starts, and I'm able to complete the Create new project dialog.  I click Finish and the dialog stays there, and nothing is create

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I cannot create a bareboard application with my new install of CodeWarrior 11.1.1 for ARM on my Ubuntu Linux system.  The IDE starts, and I'm able to complete the Create new project dialog.  I click Finish and the dialog stays there, and nothing is create

ソリューションへジャンプ
2,859件の閲覧回数
williamwatts
Contributor II

I cannot create a bareboard application with my new install of CodeWarrior 11.1.1 for ARM on my Ubuntu Linux system.  The IDE starts, and I'm able to complete the Create new project dialog.  I click Finish and the dialog stays there, and nothing is created.

ラベル(1)
1 解決策
2,724件の閲覧回数
williamwatts
Contributor II

I fixed the problem by uninstalling and reinstalling CodeWarrior.  This was for a LS1043 MCU, making an ARMv8 bareboard application.

元の投稿で解決策を見る

3 返答(返信)
2,725件の閲覧回数
williamwatts
Contributor II

I fixed the problem by uninstalling and reinstalling CodeWarrior.  This was for a LS1043 MCU, making an ARMv8 bareboard application.

2,725件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi william,

Thanks for your response, is good to hear the problem was fixed after reinstalling CodeWarrior.


Best Regards!
Carlos Mendoza
Technical Support Engineer

2,725件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee


Hi William,

Could you tell us which MCU are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer