I am using a usb tap but doesn't work on Win 7 platform. Where do I get Win 7 driver for the usb tap?  or where can I download an4338sw.zip?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am using a usb tap but doesn't work on Win 7 platform. Where do I get Win 7 driver for the usb tap?  or where can I download an4338sw.zip?

6,519 Views
BobPatton
Contributor I

I read AN4338 but there is no attachment with AN4338SW.zip needed to update usb tap driver for Win 7.

Labels (1)
4 Replies

5,725 Views
wallyqin
Contributor I

I use the tached file, it's OK!

0 Kudos
Reply

5,726 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Robert

Please download the AN4338SW.zip  attached in this thread.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

4,734 Views
Charles2053
Contributor I

Can support the 64BIT system or not?

0 Kudos
Reply

5,725 Views
wallyqin
Contributor I

thanks ,sure

0 Kudos
Reply