I am using a usb tap but doesn't work on Win 7 platform. Where do I get Win 7 driver for the usb tap?  or where can I download an4338sw.zip?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I am using a usb tap but doesn't work on Win 7 platform. Where do I get Win 7 driver for the usb tap?  or where can I download an4338sw.zip?

5,112 次查看
BobPatton
Contributor I

I read AN4338 but there is no attachment with AN4338SW.zip needed to update usb tap driver for Win 7.

标签 (1)
4 回复数

4,318 次查看
wallyqin
Contributor I

I use the tached file, it's OK!

0 项奖励
回复

4,318 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Robert

Please download the AN4338SW.zip  attached in this thread.

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

3,327 次查看
Charles2053
Contributor I

Can support the 64BIT system or not?

0 项奖励
回复

4,318 次查看
wallyqin
Contributor I

thanks ,sure

0 项奖励
回复