I am trying to run a code in MPC5604B using CodeWarrior Classic IDE 2.10. But when i run the code using internal_Flash it automatically runs the code using RAM. How can i fix this?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am trying to run a code in MPC5604B using CodeWarrior Classic IDE 2.10. But when i run the code using internal_Flash it automatically runs the code using RAM. How can i fix this?

2,145 Views
nikeshbansal
Contributor I

I am trying to run a code in MPC5604B using CodeWarrior Classic IDE 2.10. But when i run the code using internal_Flash it automatically runs the code using RAM. How can i fix this?

Labels (1)
0 Kudos
Reply
2 Replies

2,032 Views
stanish
NXP Employee
NXP Employee

Hi Nikesh,

Could you describe your issue more in the detail?

Do you use a project generated by the CodeWarrior Wizard? Have you customized the project settings?

Can you attach your internal_Flash .map + .mcp files?

Also some debugger screenshots that show the problem (e.g. the debugger after internal_flash elf is loaded, and when you run/stop execution which shows execution from ram) would help us to resolve this issue.

Thanks.

Stan

0 Kudos
Reply

2,032 Views
nikeshbansal
Contributor I

Hey Stan

Thank you so much for your help. But i have resolved the issue. Thank you anyways.

0 Kudos
Reply