I am trying to run a code in MPC5604B using CodeWarrior Classic IDE 2.10. But when i run the code using internal_Flash it automatically runs the code using RAM. How can i fix this?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I am trying to run a code in MPC5604B using CodeWarrior Classic IDE 2.10. But when i run the code using internal_Flash it automatically runs the code using RAM. How can i fix this?

2,148 次查看
nikeshbansal
Contributor I

I am trying to run a code in MPC5604B using CodeWarrior Classic IDE 2.10. But when i run the code using internal_Flash it automatically runs the code using RAM. How can i fix this?

标签 (1)
0 项奖励
回复
2 回复数

2,035 次查看
stanish
NXP Employee
NXP Employee

Hi Nikesh,

Could you describe your issue more in the detail?

Do you use a project generated by the CodeWarrior Wizard? Have you customized the project settings?

Can you attach your internal_Flash .map + .mcp files?

Also some debugger screenshots that show the problem (e.g. the debugger after internal_flash elf is loaded, and when you run/stop execution which shows execution from ram) would help us to resolve this issue.

Thanks.

Stan

0 项奖励
回复

2,035 次查看
nikeshbansal
Contributor I

Hey Stan

Thank you so much for your help. But i have resolved the issue. Thank you anyways.

0 项奖励
回复