How to work with release buttons in MQX and PE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to work with release buttons in MQX and PE?

ソリューションへジャンプ
1,288件の閲覧回数
norbertoj
Contributor III


Hi!!!

I have some problems to understand how to get an interruption of two release buttons and call a Task to work with the interruption.

 

I created a GPIO_LDD component with two GPIO Pin in Rising Edge. I used ISR (no DMA).

 

I want to know how these interrupts can be linked to the MQX TASKS Template. I created a task with the name "Buttons_task", and this task sends messages to a Main task (Control Task). I need that buttons_task go to the stack when the button is pressed.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,165件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Norberto ,

It is not from the interrupt to call Task , While  it is init interrupt in the TASK .

I recommend you refer to the interrupt demo under MQX:  Freescale_MQX_4_2\mqx\examples\isr\build

There is also PE-mqx demo under CW : CodeWarrior_Examples\Processor_Expert\MQXLite\Kinetis

There is also a GPIO interrupt demo :

How to invoke interrupt in GPIO demo project of mqx for more then one time? 

The attachment is a guide for create MQXLITE project on CW with PE, it is the same with MQX .

Hope it helps

Alice

元の投稿で解決策を見る

2 返答(返信)
1,166件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Norberto ,

It is not from the interrupt to call Task , While  it is init interrupt in the TASK .

I recommend you refer to the interrupt demo under MQX:  Freescale_MQX_4_2\mqx\examples\isr\build

There is also PE-mqx demo under CW : CodeWarrior_Examples\Processor_Expert\MQXLite\Kinetis

There is also a GPIO interrupt demo :

How to invoke interrupt in GPIO demo project of mqx for more then one time? 

The attachment is a guide for create MQXLITE project on CW with PE, it is the same with MQX .

Hope it helps

Alice

1,165件の閲覧回数
norbertoj
Contributor III

Thank you, I could establish the interrupt.

0 件の賞賛
返信