I have jumped through all the hoops to get CW 10.6 to use my external Makefile, for KL25. This Make project builds fine when CW is not evolved.
When I do 'build all' this is the result in the console:
mingw32-make[1]: *** [build_begin] Error 1
mingw32-make: *** [all] Error 2
Is it to much to ask for CW to actually tell me what the error might be? :-(
It is not listed under the 'error' tab either.
I expect it is shell related.
The environment variable MAKESHELL is properly set so that BASH is being found, yet CW is not dealing with shell lines.
#----------------------------------------------------------------------------
# Blank line in make output spew:
$(info )
#----------------------------------------------------------------------------
#----------------------------------------------------------------------------
# If there are strange erorrs about 'f not found' this indicates that
# the MS-DOS command shell is being found rather than BASH. On
# MS-DOS/Windows set the environment variable MAKESHELL to point to
# the directory that contains BASH.
$(info SHELL = '$(SHELL)')
$(info MAKESHELL = '$(MAKESHELL)')
$(info )
#----------------------------------------------------------------------------
Results in:
SHELL = 'sh.exe'
MAKESHELL = 'J:\Apps\BASH\bin'
I'm not sure if shell lines are not executing or their results go to oblivion. Either way what CW is doing is broken:
For example:
GCCVERSION := $(shell echo `$(CC) -dumpversion`)
# ifeq "$(GCCVERSION)" "4.7.1"
# CTUNING += -mstrict-X
# else
# CTUNING += -morder1 -fno-split-wide-types -fno-inline-small-functions
# CTUNING += --combine -fwhole-program
# CDEFS += -DPROGMEM_USE
# endif
$(info )
$(info Building Target: $(TARGET_DIR)/$(TARGET) with)
$(info $(CC) version: $(GCCVERSION))
$(GCCVERSION) is not being properly filled in when run from CW.
Is there any hope here or is CW a waste of time?