How to set MC9S08QE32 uart baud rate at 115200?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set MC9S08QE32 uart baud rate at 115200?

1,232 次查看
gpd
Contributor I

Hi,

I've a big problem.

I'm trying to setup my Xbee pro module via UART by AT command.

In the datasheet the default baudrate is 115200 so I'm trying to setup my MC9S08 uart to this, but I have this ERROR message:

"Time setting failed"

 

It only let me setup at 9600... how is possible?

I've used Processor Expert to setup the components.

Please Help!

70572_70572.pngScreenshot 2015-09-01 12.09.24.png

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

1,061 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Gian Paolo,

You can get a 115200 Baudrate if you set the Internal oscillator frequency to 36 KHz and the Internal bus clock to 9.216 MHz:

pastedImage_0.png

pastedImage_2.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复