How to resolve MTB Buffer attributes error?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to resolve MTB Buffer attributes error?

3,845件の閲覧回数
Embionics
Contributor III

While debugging the code, I am getting MTB Buffer Attributes error saying " Could not read MTB Buffer allocation data in elf. Trace disabled". I have checked my debug configuration, but i am clueless, how to solve this error. I am attaching the code and the snapshot of the error. Kindly help me in solving this error

Original Attachment has been moved to: LDR_Sensor_Code.rar

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

3,607件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Amreen,

Unfortunately I can not import the project.

The project is unusable.

To investigate the problem can you provide us more details:

      - what is the tool version ?

            MCU V10.?

      - zip your project folder.

I don't find lot of info / issue with MTB buffer.

Now you can have a look to:

      https://community.freescale.com/message/387709#387709

    Re: USBDM - Version 4.10.4 (RS08/HCS08/HCS12/CFV1/Kinetis BDM)


Have a great day,
Pascal

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,607件の閲覧回数
Embionics
Contributor III

Hi Pascal,

thanks for your reply.

I have recreated the project, now that error is not shown. It seems to be problem was with project properties.

0 件の賞賛
返信