How to import an existing CW project into subversion using subversive plugin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to import an existing CW project into subversion using subversive plugin?

1,693 Views
richardunruh
Contributor I

I'm running CW 10.6. I have installed the Subversive plugins from the Subversive-1.0.0.I20130122-1700.zip archive and added the Polarion SVN connectors, then added the repository location. Everything seems happy, but I can't for the life of me figure out how to import my existing CW project into subversion using the subversive plugin. Can someone point me in the right direction?? Even if it's "RTFM" and a page number.

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,521 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Richard,

- There is a User guide about using SVN on KDS, while I think it is the same with CW10.6:

Getting started with SVN and Kinetis Design Studio 

For you have install SVN , so you only needcheck the part of "4. Using version control" .

- There also a Lab about using vesrsion control on CW:

Subversion (SVN) Codewarrior 10 

pastedImage_1.png


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply