How to import an existing CW project into subversion using subversive plugin?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to import an existing CW project into subversion using subversive plugin?

1,689件の閲覧回数
richardunruh
Contributor I

I'm running CW 10.6. I have installed the Subversive plugins from the Subversive-1.0.0.I20130122-1700.zip archive and added the Polarion SVN connectors, then added the repository location. Everything seems happy, but I can't for the life of me figure out how to import my existing CW project into subversion using the subversive plugin. Can someone point me in the right direction?? Even if it's "RTFM" and a page number.

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,517件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Richard,

- There is a User guide about using SVN on KDS, while I think it is the same with CW10.6:

Getting started with SVN and Kinetis Design Studio 

For you have install SVN , so you only needcheck the part of "4. Using version control" .

- There also a Lab about using vesrsion control on CW:

Subversion (SVN) Codewarrior 10 

pastedImage_1.png


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信