How to convert XET256 banked S19 to linear by SRecCvt in command line mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to convert XET256 banked S19 to linear by SRecCvt in command line mode?

1,358件の閲覧回数
weiweichuo
Contributor I

Hi, everyone,

 

I try some command like this:

sreccvt -b 16 0xE0 -o LinearOutFile.S19 Project.abs.s19

 

there is an error code 23:

 

SRecCvt v1.0.29

 

 

Converting S-Record File: Project.abs.s19

 

 

S2247F7F00FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFC545C545C545C545C545C545C545C5459D

Error:(23) Invalid Bank Load Address

 

What should I do?

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,212件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

How does it work if with GUI mode?

can you please send me your s19 file for our testing?

Thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信