How to change the workspace name of CodeWarrior(V10.5)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change the workspace name of CodeWarrior(V10.5)?

ソリューションへジャンプ
3,275件の閲覧回数
PeterTsai
Contributor II

I have built a project in workspace. and I rename the workspace(directory) name. then open the new workspace name. but it show "Invalid workspace in use" message. May I rename the worksapce name?

 

Peter Tsai

ラベル(1)
1 解決策
2,498件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Peter

A workaround is to copy the old workspace folder, then name the new folder and delete the “.metadata” subfolder under it.

The open CodeWarrior v10.5, and click on <File> menu->Switch Workspace to select the new folder.

But you need to drag the project or import in to the CodeWarrior Project view. The old project view is not kept.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,499件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello Peter

A workaround is to copy the old workspace folder, then name the new folder and delete the “.metadata” subfolder under it.

The open CodeWarrior v10.5, and click on <File> menu->Switch Workspace to select the new folder.

But you need to drag the project or import in to the CodeWarrior Project view. The old project view is not kept.

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------