How to change color theme tp dark in CodeWarrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change color theme tp dark in CodeWarrior

9,866 Views
marceli1
Contributor III

I need to change color theme in CodeWarrior like VisualStudio2017 has. Is any way do it?

Labels (1)
4 Replies

8,766 Views
marceli1
Contributor III

Thank you, it was helpful. Still need to learn use MCU Express It is not so fast as Processor Express in CW.

0 Kudos
Reply

8,766 Views
BlackNight
NXP Employee
NXP Employee

You can change the Theme here:

pastedImage_1.png

But you won't get a 'dark' theme. For this you need a more recent Eclipse version. Not sure what device/microcontroller you are using. I suggest you use the MCUXpresso IDE which supports dark and darkest themes (see Installing Darkest Theme with MCUXpresso IDE 10.2 | MCU on Eclipse which describes it for 10.2). The current MCUXpresso IDE is 10.3.0 and comes with the Dark Theme pre-installed:

pastedImage_3.png

I hope this helps,

Erich

8,766 Views
jpotter
Contributor I

I get the same error when I try and install mynlyn before as you saw when you attempted to install devstyle.... codewarrior DS 11.1

0 Kudos
Reply

8,766 Views
bart1
Contributor II

I am having the same problem with cw ds 11.1, have you found a solution yet?

working in a dark room with the white screen is killing my eyes(windows night light does help a bit).