How to change color theme tp dark in CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change color theme tp dark in CodeWarrior

9,706件の閲覧回数
marceli1
Contributor III

I need to change color theme in CodeWarrior like VisualStudio2017 has. Is any way do it?

ラベル(1)
4 返答(返信)

8,606件の閲覧回数
marceli1
Contributor III

Thank you, it was helpful. Still need to learn use MCU Express It is not so fast as Processor Express in CW.

0 件の賞賛
返信

8,606件の閲覧回数
BlackNight
NXP Employee
NXP Employee

You can change the Theme here:

pastedImage_1.png

But you won't get a 'dark' theme. For this you need a more recent Eclipse version. Not sure what device/microcontroller you are using. I suggest you use the MCUXpresso IDE which supports dark and darkest themes (see Installing Darkest Theme with MCUXpresso IDE 10.2 | MCU on Eclipse which describes it for 10.2). The current MCUXpresso IDE is 10.3.0 and comes with the Dark Theme pre-installed:

pastedImage_3.png

I hope this helps,

Erich

8,606件の閲覧回数
jpotter
Contributor I

I get the same error when I try and install mynlyn before as you saw when you attempted to install devstyle.... codewarrior DS 11.1

0 件の賞賛
返信

8,606件の閲覧回数
bart1
Contributor II

I am having the same problem with cw ds 11.1, have you found a solution yet?

working in a dark room with the white screen is killing my eyes(windows night light does help a bit).