How to buy codewarrior basic perpetual with node locked dongle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to buy codewarrior basic perpetual with node locked dongle

1,693 Views
wallywillemse
Contributor I

How to purchase codewarrior basic with Processor expert, version 10.7 or thereabouts, perpetual license but node locked through a dongle?

Wally e-mail: [email protected] or cell: (858) 663 5772. 

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,571 Views
TomasPaez
NXP Employee
NXP Employee

Check the following link on the cost of the CodeWarrior suite, There are 3 options, BASIC , STANDARD and PRO. If you need to use Processor Expert, the PRO is the option with all PE components.

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to...

Dongle use, can be avoided since the license system allows you to move between station by updating the host information.

CWH-DONGLE is the part number you can get in case this is needed. Hope this helps.

0 Kudos
Reply

1,572 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Wally,

To order a dongle-based license, order the node-locked option for your CodeWarrior suite and also order the USB licensing dongle (CWH-DONGLE).

Refer to your requirement choose CodeWarrior suite :

CodeWarrior Embedded Software Development Tools|NXP 


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply