How do I program the MC9S08SH8? What hardware to do I need to program and what software should I use to program?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I program the MC9S08SH8? What hardware to do I need to program and what software should I use to program?

2,380件の閲覧回数
pmchoudek
Contributor I

I am thinking of using the MC9S08SH8 microprocessor for a school project.  I need to know how to program it.  I have used ST-link V2 programmer to program a different chip: LPC1114 DIP package.  When I did that I used the Keil Arm-Core program to flash-program my chip.

How would I program this chip?  Is there something like the ST link V2 I have to buy?  What software do I need to have to program this?  Is Keil microvision acceptable?  

I have the datasheet pulled up on my computer and I would be getting the 20 pin PDIP package for this project.  I am not sure which pins I have to use to program it.  I remember connecting the SWDIO pin on the LPC1114 with the ST-Link V2.

I also would like to know if there are any header files I need to include in my programming to make sure the microprocessor is set up correctly.  

If there is any help you could give me on this, I would be truly appreciative.

Thank you,

Peter

タグ(1)
0 件の賞賛
返信
1 返信

2,281件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Peter,

For SH8, our recommended debug probe is Multilink:

MULTILINK | Debug Probe | PEmicro 

our recommended IDE is CodeWarrior 11

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t... 


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信