Required MC56F8367 header files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Required MC56F8367 header files

ソリューションへジャンプ
2,516件の閲覧回数
padmaashok765
Contributor II

Hi,

To program mc56f8367 i'm using CodeWarrior v8.3. I need header files and a simple program to initialize TXD0 using that header file.  

what is the default header file for mc56f8367?

Thanks in advance

ラベル(1)
タグ(3)
1 解決策
2,430件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

If you have CW11 installed, you will find MC56F8367 header files under CW install folder.

I attach it here for your convenience.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
2,431件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

If you have CW11 installed, you will find MC56F8367 header files under CW install folder.

I attach it here for your convenience.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,430件の閲覧回数
padmaashok765
Contributor II

Thankyou Jun Zhang

0 件の賞賛
返信
2,430件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 件の賞賛
返信