How can I find corresponding CWH part number for 900-75115; REV E?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I find corresponding CWH part number for 900-75115; REV E?

Jump to solution
3,111 Views
spmsale
Contributor II

How can I find corresponding CWH part number for 900-75115; REV E?

Labels (1)
1 Solution
2,829 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Manoj

The part number of your USBTAP is CWH-UTP-PPCC-HE. It is designed for PowerPC targets. 

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

6 Replies
2,594 Views
Pradeepkumar_S
Contributor II

One quick question.. Does this TAP support MPC870 Processor.

Regards

Pradeep. S

0 Kudos
Reply
2,829 Views
spmsale
Contributor II

Hello Xin,

Thank you very much for your prompt response. The characters are COP.

Thank you,

Manoj

0 Kudos
Reply
2,830 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Manoj

The part number of your USBTAP is CWH-UTP-PPCC-HE. It is designed for PowerPC targets. 

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,829 Views
spmsale
Contributor II

Thank you for the information.

Another question is, what are the differences between different Rev?

For Example:

Rev C

Rev D

Rev G

Thank you,

Manoj

0 Kudos
Reply
2,829 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Manoj

There are some improvements on hardware design between different reversions, especially to minimize ESD harming.

For example, Rev E introduced a hardware redesign, but maintains complete software and firmware compatibility.  The goal was a more robust USBTAP which could better handle unwanted static discharges, and better shielded from electromagnetic interference.

Release notes from Rev E:

  • Software compatible with existing UTAPS (no need for CodeWarrior upgrade)
  • Converted USB Type B connector to a USB Micro B connector (this will minimize ESD harming the unit)
  • More robust target cable (this will reduce susceptibility to EMI)
  • Plastic Case (this will minimize ESD harming the unit)

Rev F fixed one specific electrical issue with on flavor on PA processors introduced in the Rev E redesign. 

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 Kudos
Reply
2,829 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Monoj

We have several types of USBTAP for different products. Please look at bottom on UTAP case. The sticker on the bottom of the case will show ONCE, COP, CF…. please supply with these characters.

Best Regards

Fiona Kuang

TIC - Technical Information Center

0 Kudos
Reply