How Can I install CodeWarrior V6.3. on a Win7 64 bit computer?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How Can I install CodeWarrior V6.3. on a Win7 64 bit computer?

1,885 次查看
jungwoojin
Contributor I

when i installed the CW v6.3, i can see the warning message about " CodeWarrior development studio for microcontrollers v6.3 is not compatible with Windows XP 64-bit installation."

 

 

Please tell me how to install the CW v6.3 in windows7 64bit.

 

Or, please tell the program to replace the CW v6.3.

 

MCU is 'S9S08AW16AMLD'

标签 (1)
0 项奖励
回复
1 回复

1,469 次查看
trytohelp
NXP Employee
NXP Employee

Hi,

Please have a look to the message:

    Install CodeWarrior 6.3 Windows 7 & 10 x64 directly (Classic version)

Scroll down to have all information and option to install the CW for MCU v6.3 on Win 7 and higher version.


Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复