Help- using Integrated USB BDM of M52233Demo with CW10.5IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help- using Integrated USB BDM of M52233Demo with CW10.5IDE

1,046件の閲覧回数
pavanbg
Contributor I

Hello ,

 

I am using Codewarrior 10.5 Eclipse for MCUs on Win7 , I have a M52233Demo board and I want to use the Integrated USB BDM  with CW10.5 ,I have done the hardware jumper settings please help me with the configuration in CW10.5 .Thanks

 

Regards

Pavan

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

935件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

we were ever informed by P&E that BDM Modules are low cost BDM modules that are not intended to be used for anything else other than program the device present on the demoboard. Even attempting to program the same derivative part number but on an external target is not guaranteed it will work.  P&E does not support this and Freescale support should not assist customers who try to hack these boards to turn them into programmers.

hope this information can make sense for you.

----------------------------------------------------------------

this answer is for you. if this helps, please click on "correct answer" button. thanks!

Best Regards,

ZhangJun

0 件の賞賛
返信