Hello, I'm Reinhold

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello, I'm Reinhold

5,605 Views
reinholdglatz
Contributor I

I refere to this Freescale file relating a so called "Digibutle kit" hardware platform ...

 

http://www.freescale.com/files/microcontrollers/doc/support_info/DIGIBUTLER_2.pdf

 

... and there in page 2 of 6  ...

 

"Compilation and (re)flashing the MCF52231 requires

CodeWarrior Development Studio for Coldfire Architectures, v. 6.3.

CodeWarrior is an integrated development environment which includes a project manager, editor, compiler and debugger.

Version 6.3 is a free download.

At ref. [1] it’s marked as “Updates and Patches” but Elektor has ‘inside information’ that it’s actually a full install version!

The download is about 140 MB. "

 

I am a teacher at => http://www.HTL-donaustadt.at 

Tw of my students need to recompile Eric Gregory's (=>Freescale) Code for the "DigiButler kit" in order to extend the "Digibutle kit" firmware functionality.

 

The reference [1] as given in the file mentioned above does not land at freescale webpage any more.

 

Questions 1: is the page titeled "CodeWarrior for Microcontrollers (Classic IDE) - RS08/HC(S)08, ColdFire V1 v6.3 "

 

see link...

 

CodeWarrior for Microcontrollers-Classic IDE|Freescale

 

... the web site in order to donwload the ...

 

"CodeWarrior Development Studio for Coldfire Architectures, v. 6.3."

 

... as mentioned in the PDF-File?

 

Questions 2: If so, and having a look at web site ...

 

https://freescale.flexnetoperations.com/control/frse/download?element=5901331

...

 

wich of the 13 files shall I download in order to get the CW IDE as needed for freescales MCU with part number "MCF52231"

(i.e. the MCU residing at the traget "Digibutle kit")?

 

Questions 3: Further more, we want to flash the target "Digibutle kit"(=> it supports a 26 pin Coldfire BDM port)  with the "USB-ML-UNIVERSAL"; this programmer device I've  ordered and (already) received from "P&E Microcumputer Systems, Inc." (=> www.pemicro.com).

Will the "CodeWarrior for Microcontrollers (Classic IDE) - RS08/HC(S)08, ColdFire V1 v6.3 " support the "USB-ML-UNIVERSAL" programmer.

 

Thx for help in advance,

and best regards,

 

Reinhold.

web: http://www.htl-donaustadt.at

eMail: [email protected]

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

5,060 Views
trytohelp
NXP Employee
NXP Employee

another point ...

More details for question 3.

2 weeks ago I've posted a feedback about that under the Thread:

      Install CodeWarrior v6.3 directly under Windows 7 x64

Extract of feedback:

++++++++++++++++++++++++

've performed some tests on my side.

My config is:

  Software:

      Windows 7 64 bit

      CW for MCU V6.3 + P&E driver version 11

      CW for MCU V10.6

  Hardware:

      TWR-S08UNIV + TWR-S08DC-AC60

      USB Multilink HCS08/HCS12 (USB-ML-12) rev B

      USB Multilink Universal (USB-ML-UNIVERSAL) rev B

Test_1:

I've created a project under MCU V10.6 for Mulitlink interface.

Under MCU V10.6 the 2 interfaces are running without problem.

Test_2:

I've create a project under MCU V6.3 for Multilink interface.

In this situation the interface are not running.

How to solve the problem ?

Refer to the FAQ P&E Microcomputer Systems

I've downloaded the CW63_patch_S08.RS08.CFV1.zip.

A ReadMe.txt file explains step by step the process to follow.

I did:

1. Close any running CodeWarrior applications.

2. Search the CodeWarrior application directory for the prog/P&E folder.

3. When the directory is located, make a copy of the P&E folder and rename it to P&E.backup or archive it so you can restore it at a later time if necessary.

4. Merge all files from the patch into the prog/P&E directory.

5. Restart the application debugger and try to debug your target board.

Now with the 2 interfaces under MCU V6.3, I can load the application on board.

++++++++++++++++++++++++


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,060 Views
trytohelp
NXP Employee
NXP Employee

Hi Reinhold,

There are several tools products:

      Classic version and Eclipse version

The Eclipse version is the new one based on Eclipse IDE.

The last version is CW for MCU V10.6.

It integrates the development tools for the :

                ColdFire®, ColdFire+, DSC, Kinetis, Qorivva, RS08, S08 and S12Z architectures

into a single product based on the Eclipse open development platform.

This version is running on Host platforms

                Microsoft® Windows XP 32-bit and 64-bit (Professional Edition)

                Microsoft Windows 7 32-bit and 64-bit (Home Premium Edition and Professional Edition)

                Microsoft Windows 8 32-bit and 64-bit (Home Premium Edition and Professional Edition)

You can download an evaluation on the web site:

                http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10

The tools you referred are based on Classic IDE (older version).

2 development tools are supporting Coldfire Architectures.

A- CodeWarrior for Microcontrollers (Classic IDE) - RS08/HC(S)08, ColdFire V1 v6.3

            http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MICROCONTROLLERS&tid=CWH

      Freescale's CodeWarrior Development Studio for Microcontrollers v6.3 is a single, integrated tool suite designed to get you on the design fast track with RS08, S08 and ColdFire V1

B- CodeWarrior Development Studio for ColdFire Architectures (Classic IDE) v7.2

            CodeWarrior Development Tools for ColdFire|Freescale

      CodeWarrior Development Studio for ColdFire Architectures v7.2 is a single, integrated tool suite designed to get you on the design fast track with ColdFire V2, V3, V4 and V4e

To resume:

Coldfire V1 was not included in CW development tool dedicated to Coldfire Architecture but was included in the S08 development tool.

CW for Coldfire V6.3 is an older version of CW for Coldfie V7.2.

To answer your questions:

1- No. CW for MCU V6.3 and CW for Coldfire V6.3 are 2 different tools.

2- Sorry but I can not access to the link.

3- To avoid problem we recommend to use the last version which is CW for MCU V10.6.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,059 Views
reinholdglatz
Contributor I

Hi Pascal and thx for Your feedback.

You wrote … “2- Sorry but I can not access to the link.” … , i.e. relating the URL in my

“Questions 2: If so, and having a look at web site ...”

In order to open it …

1st => open link …

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MICROCONTROLLERS

..then push “download” button.

2nd => sign in

3rd => push the “I Agree” button …

4th => … the 13 files (as I mentioned) to download are seen …

My bee, You are then able to also answer my “Questions 2”? ☺

What are all these 13 files to used for ? … and …

… does this IDE package really not support Freescales “"MCF52231" controller?

Thx in advance, greetings from Vienna Austria and …

Best Regards,

Reinhold

Von: Pascal Irrle

Gesendet: Dienstag, 24. Februar 2015 12:34

An: GLATZ, Reinhold

Betreff: Re: - Hello, I'm Reinhold

<https://community.freescale.com/>

Hello, I'm Reinhold

reply from Pascal Irrle<https://community.freescale.com/people/trytohelp?et=watches.email.thread> in CodeWarrior Development Tools - View the full discussion<https://community.freescale.com/message/483811?et=watches.email.thread#483811>

0 Kudos
Reply

5,059 Views
trytohelp
NXP Employee
NXP Employee

Reinhold,

The tool you're looking for is CW for MCU V6.3.

This tool is supporting RS08/HC0/HCS08 and Coldfire V1 Architectures.

MCF52231 is a Coldfire V2 and so not supported by CW for MCU V6.3.

What about the 13 files listed here ?

      - there is the installer which is the tool base,

      - there are 10 service packs.

            A service pack must be apply to support a specific processor which was not supported in the tool base.

      - 2 software patches including new development tool as compiler update, etc ...

What are the tools supporting MCF52xxx ?

2 solutions:

          - Classic version: CW for Coldfire V7.2 or V2.5

                for windows OS:    CodeWarrior Development Tools for ColdFire|Freescale

                for linux OS:          CodeWarrior Dev Tools for ColdFire: Linux|Freescale

          - Eclipse:      CW for MCU V10.6

              for windows and linux os: CodeWarrior for Microcontrollers-Eclipse IDE|Freescale

My recommendation.

for new project I recommend you to install and use the Eclipse version.

This was released in 2014 and it's the most recent version.

The Classic version CW for Coldfire V7.2 was released in 2010.

Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

5,059 Views
reinholdglatz
Contributor I

Pascal,

let me at least feedback a „thank You“ for Your most professional expertise!

Best Regards from Vienna Austria,

Reinhold.

Von: Pascal Irrle

Gesendet: Mittwoch, 25. Februar 2015 08:09

An: GLATZ, Reinhold

Betreff: Re: - Hello, I'm Reinhold

<https://community.freescale.com/>

Hello, I'm Reinhold

reply from Pascal Irrle<https://community.freescale.com/people/trytohelp?et=watches.email.thread> in CodeWarrior Development Tools - View the full discussion<https://community.freescale.com/message/484174?et=watches.email.thread#484174>

0 Kudos
Reply