HCS12X-How does DFLASH differ from EEPROM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS12X-How does DFLASH differ from EEPROM?

Jump to solution
4,781 Views
AndersJ
Contributor IV

In most litterature and in Processor Expert the term EEPROM is used.

Sometimes however, the term DFLASH is also used.

The PE-Micro Cyclone PRO programmer has EEPROM and DFLASH programming algoritms,

suggesting that there are two different memory types.

 

What is the difference between EEPROM and DFLASH?

Labels (1)
0 Kudos
Reply
1 Solution
3,624 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Earlier S12 and S12X microcontrollers contained standard EEPROM memory. The main characteristic (from the user’s point of view) is that the sector size is 4 bytes (smallest partition of memory that can be erased).

 

Microcontrollers from S12XE and S12XF family are a little bit different. The technology has been changed – the memory size is higher but also the sector has been increased to 256 bytes. This kind of EEPROM memory is called D-Flash.

 

There are two ways to access this memory.

The user can work with the D-Flash directly – through the standard flash commands like “Program D-Flash Command”, “Erase D-Flash Sector Command”…

 

The next possibility is usage of Emulated EEPROM. What does it mean – the user just reads/writes data from/to Buffer RAM. The internal mechanism will ensure the data integrity between Buffer RAM and D-Flash. It automatically loads data from D-Flash to Buffer RAM after reset and automatically stores the data to D-Flash when writing to Buffer RAM. So, it’s very comfortable for user because he can use the EEPROM memory which behaves like RAM memory.

 

This is only short description, I recommend the application note AN3490 where is the complete explanation.

 

http://www.freescale.com/files/microcontrollers/doc/app_note/AN3490.pdf


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
3,625 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Earlier S12 and S12X microcontrollers contained standard EEPROM memory. The main characteristic (from the user’s point of view) is that the sector size is 4 bytes (smallest partition of memory that can be erased).

 

Microcontrollers from S12XE and S12XF family are a little bit different. The technology has been changed – the memory size is higher but also the sector has been increased to 256 bytes. This kind of EEPROM memory is called D-Flash.

 

There are two ways to access this memory.

The user can work with the D-Flash directly – through the standard flash commands like “Program D-Flash Command”, “Erase D-Flash Sector Command”…

 

The next possibility is usage of Emulated EEPROM. What does it mean – the user just reads/writes data from/to Buffer RAM. The internal mechanism will ensure the data integrity between Buffer RAM and D-Flash. It automatically loads data from D-Flash to Buffer RAM after reset and automatically stores the data to D-Flash when writing to Buffer RAM. So, it’s very comfortable for user because he can use the EEPROM memory which behaves like RAM memory.

 

This is only short description, I recommend the application note AN3490 where is the complete explanation.

 

http://www.freescale.com/files/microcontrollers/doc/app_note/AN3490.pdf


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------