Freescale USB TAP box grayed out - HELP!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Freescale USB TAP box grayed out - HELP!

跳至解决方案
2,632 次查看
Steve_AIMMS
Contributor I

I am using CW11.1 for DSC on Win 7.  I have successfully (based on window's responses) installed the USB TAP driver from the CW 11.1 installation's subfolder \MCU\ccs\drivers\usb.  I rebooted the machine and then created a new DSC project for the 56F83783 processor.  From the Connections form after selecting New Bareboard Project, I see the list of possible connections and "Freescale USB TAP" is grayed out.  Why can't I select this option? Is it a hardware incompatibility and I have to find another way to JTAG debug or is it a problem with software configuration still?  

Thanks!

0 项奖励
回复
1 解答
2,624 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Stephen,

For the latest MC56F83xxx, MC56F81xxx and future DSC family, the USBTAP device is NOT supported, user can use the third party device for example Multilink Universal device from PE micro.

http://www.pemicro.com/

Hope it can help you

BR

XiangJun Rong

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,625 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Stephen,

For the latest MC56F83xxx, MC56F81xxx and future DSC family, the USBTAP device is NOT supported, user can use the third party device for example Multilink Universal device from PE micro.

http://www.pemicro.com/

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复
2,529 次查看
rosendalin
Contributor I

Thanks for your answer. It helped me a lot.

0 项奖励
回复