Freescale USB TAP box grayed out - HELP!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale USB TAP box grayed out - HELP!

ソリューションへジャンプ
2,588件の閲覧回数
Steve_AIMMS
Contributor I

I am using CW11.1 for DSC on Win 7.  I have successfully (based on window's responses) installed the USB TAP driver from the CW 11.1 installation's subfolder \MCU\ccs\drivers\usb.  I rebooted the machine and then created a new DSC project for the 56F83783 processor.  From the Connections form after selecting New Bareboard Project, I see the list of possible connections and "Freescale USB TAP" is grayed out.  Why can't I select this option? Is it a hardware incompatibility and I have to find another way to JTAG debug or is it a problem with software configuration still?  

Thanks!

0 件の賞賛
返信
1 解決策
2,580件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Stephen,

For the latest MC56F83xxx, MC56F81xxx and future DSC family, the USBTAP device is NOT supported, user can use the third party device for example Multilink Universal device from PE micro.

http://www.pemicro.com/

Hope it can help you

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,581件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Stephen,

For the latest MC56F83xxx, MC56F81xxx and future DSC family, the USBTAP device is NOT supported, user can use the third party device for example Multilink Universal device from PE micro.

http://www.pemicro.com/

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信
2,485件の閲覧回数
rosendalin
Contributor I

Thanks for your answer. It helped me a lot.

0 件の賞賛
返信