Freemaster 2.0 problems to generate a two-dimensional array variables

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freemaster 2.0 problems to generate a two-dimensional array variables

Jump to solution
4,092 Views
mirkoruggeri
Contributor II

Hi,

I tried to generate the visualization of two-dimensional array variables in Freemaster 2.0.0.10 and in 2.0.2, but this is not possible.

 

I already use the same two-dimensional array in Fremaster 1.3 and it can show the array correctly.

 

How can I visualize a two dimensional array in Freemaster 2.0?

 

Many Thanks.

Mirko

Labels (1)
0 Kudos
Reply
1 Solution
3,928 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mirko,

Yes, there is some difference between the two version.

In Freemater v2.0,  for example i define a two-dimensional array variables test[2][2];

Please refer to the screenshots below :

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

This process add the test[0][2] to watch.

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
5 Replies
3,928 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mirko,

Could you please describe your question more detail ?

What is look like about "a two dimensional array " in the Freemaster 1.3 ?

Please share the screenshot about the array in Freemater 1.3, and i refer to it

to check whether the V2.0 has the same function.

BR

Alice

0 Kudos
Reply
3,928 Views
mirkoruggeri
Contributor II

Hello Alice,

I have an array like this

2016-12-19_085527.JPG

If I try to show the array with Freemaster 1.3 I can chose between the 2 index of array

2016-12-19_085847_b.JPG

For the same array, in Freemaster 2.0 I can't able to chose the 2 index.

2016-12-19_090126_b.JPG

Best Regards

Mirko

0 Kudos
Reply
3,929 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mirko,

Yes, there is some difference between the two version.

In Freemater v2.0,  for example i define a two-dimensional array variables test[2][2];

Please refer to the screenshots below :

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

This process add the test[0][2] to watch.

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,928 Views
mirkoruggeri
Contributor II

Hello Alice.

Yes, I solved using your suggestion.

In detail... I created an array for each single element of the first index of the array.

2016-12-19_134525.JPG

2016-12-19_134629.JPG

2016-12-19_134916.JPG

FM13.JPG

FM20.JPG

In my opinion the method offered by Freemaster 1.3 is more "user friendly", anyway the workaround suggested properly solve the problem.

Many Thanks for your answer.

Best Regards

Mirko

0 Kudos
Reply
3,928 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mirko,

Also thanks for you sharing it , thanks!

BR

Alice

0 Kudos
Reply