Flash memory map conflict between documentation and template P2020RDB-PCA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash memory map conflict between documentation and template P2020RDB-PCA

2,684 次查看
felipe-gm
Contributor II

Hi there,

I am new to working with PowerPC P2020 dev board and its ecosystem. Still, I have worked with another PPC family before, the MPC 5777C dev board. I will try to go into details of my problem.

Currently, I am stating to develop applications for WindRiver's VxWorks, using their Workbench application. They provided me with the BSP file for my target, the P2020RDB board. The board has U-boot installed by default. 

Now, my problem here is with the flash mapping. NXP documentation shows the flash memory mapped to addresses between 0xEF000000 to 0xEFFFFFFF (16 mb) as:

pastedImage_1.png

U-Boot executing on the target, provides the same information (please notice flashstart and size):

pastedImage_2.png

On the other hand, NXP Codewarrior template for the target, as well as WindRiver BSP files, point to a different Flash memory mapping: from 0xFF000000 to 0xFFFFFFFF - and hence the same 16mb, but shifted. 

VxWorks mapping:

pastedImage_6.png

Codewarrior diagnostics:

l::target -lc "P2020-RDB-core00_RAM_P2020_Connect"
fl::target -b 0x0 0x40000000
fl::target -v on -l off
cmdwin::fl::device -d "S29GL128P" -o "8Mx16x1" -a 0xff000000 0xffffffff
cmdwin::fl::diagnose full
 Beginning Operation ...   
-------------------------
Performing target initialization ...   
 Downloading Flash Diagnostics Driver ...  
 Reading flash ID ...
Running Diagnostics ...  
 Running Diagnostics ........
Sector Map (read from target)  
=============================  
Sector 00000: 0xFF000000 - 0xFF01FFFF Size=0x00020000 unprotected programmed  
Sector 00001: 0xFF020000 - 0xFF03FFFF Size=0x00020000 unprotected      blank  
Sector 00002: 0xFF040000 - 0xFF05FFFF Size=0x00020000 unprotected programmed  
Sector 00003: 0xFF060000 - 0xFF07FFFF Size=0x00020000 unprotected      blank  
Sector 00004: 0xFF080000 - 0xFF09FFFF Size=0x00020000 unprotected programmed  
Sector 00005: 0xFF0A0000 - 0xFF0BFFFF Size=0x00020000 unprotected programmed  
Sector 00006: 0xFF0C0000 - 0xFF0DFFFF Size=0x00020000 unprotected programmed  
Sector 00007: 0xFF0E0000 - 0xFF0FFFFF Size=0x00020000 unprotected programmed  
Sector 00008: 0xFF100000 - 0xFF11FFFF Size=0x00020000 unprotected programmed  
Sector 00009: 0xFF120000 - 0xFF13FFFF Size=0x00020000 unprotected programmed  
Sector 00010: 0xFF140000 - 0xFF15FFFF Size=0x00020000 unprotected programmed  
Sector 00011: 0xFF160000 - 0xFF17FFFF Size=0x00020000 unprotected programmed  
Sector 00012: 0xFF180000 - 0xFF19FFFF Size=0x00020000 unprotected programmed  
Sector 00013: 0xFF1A0000 - 0xFF1BFFFF Size=0x00020000 unprotected programmed  
Sector 00014: 0xFF1C0000 - 0xFF1DFFFF Size=0x00020000 unprotected programmed  
Sector 00015: 0xFF1E0000 - 0xFF1FFFFF Size=0x00020000 unprotected programmed  
Sector 00016: 0xFF200000 - 0xFF21FFFF Size=0x00020000 unprotected programmed  
Sector 00017: 0xFF220000 - 0xFF23FFFF Size=0x00020000 unprotected programmed  
Sector 00018: 0xFF240000 - 0xFF25FFFF Size=0x00020000 unprotected programmed  
Sector 00019: 0xFF260000 - 0xFF27FFFF Size=0x00020000 unprotected programmed  
Sector 00020: 0xFF280000 - 0xFF29FFFF Size=0x00020000 unprotected programmed  
Sector 00021: 0xFF2A0000 - 0xFF2BFFFF Size=0x00020000 unprotected programmed  
Sector 00022: 0xFF2C0000 - 0xFF2DFFFF Size=0x00020000 unprotected programmed  
Sector 00023: 0xFF2E0000 - 0xFF2FFFFF Size=0x00020000 unprotected programmed  
Sector 00024: 0xFF300000 - 0xFF31FFFF Size=0x00020000 unprotected programmed  
Sector 00025: 0xFF320000 - 0xFF33FFFF Size=0x00020000 unprotected programmed  
Sector 00026: 0xFF340000 - 0xFF35FFFF Size=0x00020000 unprotected programmed  
Sector 00027: 0xFF360000 - 0xFF37FFFF Size=0x00020000 unprotected programmed  
Sector 00028: 0xFF380000 - 0xFF39FFFF Size=0x00020000 unprotected programmed  
Sector 00029: 0xFF3A0000 - 0xFF3BFFFF Size=0x00020000 unprotected programmed  
Sector 00030: 0xFF3C0000 - 0xFF3DFFFF Size=0x00020000 unprotected programmed  
Sector 00031: 0xFF3E0000 - 0xFF3FFFFF Size=0x00020000 unprotected programmed  
Sector 00032: 0xFF400000 - 0xFF41FFFF Size=0x00020000 unprotected programmed  
Sector 00033: 0xFF420000 - 0xFF43FFFF Size=0x00020000 unprotected programmed  
Sector 00034: 0xFF440000 - 0xFF45FFFF Size=0x00020000 unprotected programmed  
Sector 00035: 0xFF460000 - 0xFF47FFFF Size=0x00020000 unprotected programmed  
Sector 00036: 0xFF480000 - 0xFF49FFFF Size=0x00020000 unprotected programmed  
Sector 00037: 0xFF4A0000 - 0xFF4BFFFF Size=0x00020000 unprotected programmed  
Sector 00038: 0xFF4C0000 - 0xFF4DFFFF Size=0x00020000 unprotected programmed  
Sector 00039: 0xFF4E0000 - 0xFF4FFFFF Size=0x00020000 unprotected programmed  
Sector 00040: 0xFF500000 - 0xFF51FFFF Size=0x00020000 unprotected programmed  
Sector 00041: 0xFF520000 - 0xFF53FFFF Size=0x00020000 unprotected programmed  
Sector 00042: 0xFF540000 - 0xFF55FFFF Size=0x00020000 unprotected programmed  
Sector 00043: 0xFF560000 - 0xFF57FFFF Size=0x00020000 unprotected programmed  
Sector 00044: 0xFF580000 - 0xFF59FFFF Size=0x00020000 unprotected programmed  
Sector 00045: 0xFF5A0000 - 0xFF5BFFFF Size=0x00020000 unprotected programmed  
Sector 00046: 0xFF5C0000 - 0xFF5DFFFF Size=0x00020000 unprotected programmed  
Sector 00047: 0xFF5E0000 - 0xFF5FFFFF Size=0x00020000 unprotected programmed  
Sector 00048: 0xFF600000 - 0xFF61FFFF Size=0x00020000 unprotected programmed  
Sector 00049: 0xFF620000 - 0xFF63FFFF Size=0x00020000 unprotected programmed  
Sector 00050: 0xFF640000 - 0xFF65FFFF Size=0x00020000 unprotected programmed  
Sector 00051: 0xFF660000 - 0xFF67FFFF Size=0x00020000 unprotected programmed  
Sector 00052: 0xFF680000 - 0xFF69FFFF Size=0x00020000 unprotected programmed  
Sector 00053: 0xFF6A0000 - 0xFF6BFFFF Size=0x00020000 unprotected programmed  
Sector 00054: 0xFF6C0000 - 0xFF6DFFFF Size=0x00020000 unprotected programmed  
Sector 00055: 0xFF6E0000 - 0xFF6FFFFF Size=0x00020000 unprotected programmed  
Sector 00056: 0xFF700000 - 0xFF71FFFF Size=0x00020000 unprotected programmed  
Sector 00057: 0xFF720000 - 0xFF73FFFF Size=0x00020000 unprotected programmed  
Sector 00058: 0xFF740000 - 0xFF75FFFF Size=0x00020000 unprotected programmed  
Sector 00059: 0xFF760000 - 0xFF77FFFF Size=0x00020000 unprotected programmed  
Sector 00060: 0xFF780000 - 0xFF79FFFF Size=0x00020000 unprotected programmed  
Sector 00061: 0xFF7A0000 - 0xFF7BFFFF Size=0x00020000 unprotected programmed  
Sector 00062: 0xFF7C0000 - 0xFF7DFFFF Size=0x00020000 unprotected programmed  
Sector 00063: 0xFF7E0000 - 0xFF7FFFFF Size=0x00020000 unprotected programmed  
Sector 00064: 0xFF800000 - 0xFF81FFFF Size=0x00020000 unprotected programmed  
Sector 00065: 0xFF820000 - 0xFF83FFFF Size=0x00020000 unprotected programmed  
Sector 00066: 0xFF840000 - 0xFF85FFFF Size=0x00020000 unprotected programmed  
Sector 00067: 0xFF860000 - 0xFF87FFFF Size=0x00020000 unprotected programmed  
Sector 00068: 0xFF880000 - 0xFF89FFFF Size=0x00020000 unprotected programmed  
Sector 00069: 0xFF8A0000 - 0xFF8BFFFF Size=0x00020000 unprotected programmed  
Sector 00070: 0xFF8C0000 - 0xFF8DFFFF Size=0x00020000 unprotected programmed  
Sector 00071: 0xFF8E0000 - 0xFF8FFFFF Size=0x00020000 unprotected programmed  
Sector 00072: 0xFF900000 - 0xFF91FFFF Size=0x00020000 unprotected programmed  
Sector 00073: 0xFF920000 - 0xFF93FFFF Size=0x00020000 unprotected programmed  
Sector 00074: 0xFF940000 - 0xFF95FFFF Size=0x00020000 unprotected programmed  
Sector 00075: 0xFF960000 - 0xFF97FFFF Size=0x00020000 unprotected programmed  
Sector 00076: 0xFF980000 - 0xFF99FFFF Size=0x00020000 unprotected programmed  
Sector 00077: 0xFF9A0000 - 0xFF9BFFFF Size=0x00020000 unprotected programmed  
Sector 00078: 0xFF9C0000 - 0xFF9DFFFF Size=0x00020000 unprotected programmed  
Sector 00079: 0xFF9E0000 - 0xFF9FFFFF Size=0x00020000 unprotected programmed  
Sector 00080: 0xFFA00000 - 0xFFA1FFFF Size=0x00020000 unprotected programmed  
Sector 00081: 0xFFA20000 - 0xFFA3FFFF Size=0x00020000 unprotected programmed  
Sector 00082: 0xFFA40000 - 0xFFA5FFFF Size=0x00020000 unprotected programmed  
Sector 00083: 0xFFA60000 - 0xFFA7FFFF Size=0x00020000 unprotected programmed  
Sector 00084: 0xFFA80000 - 0xFFA9FFFF Size=0x00020000 unprotected      blank  
Sector 00085: 0xFFAA0000 - 0xFFABFFFF Size=0x00020000 unprotected      blank  
Sector 00086: 0xFFAC0000 - 0xFFADFFFF Size=0x00020000 unprotected      blank  
Sector 00087: 0xFFAE0000 - 0xFFAFFFFF Size=0x00020000 unprotected      blank  
Sector 00088: 0xFFB00000 - 0xFFB1FFFF Size=0x00020000 unprotected      blank  
Sector 00089: 0xFFB20000 - 0xFFB3FFFF Size=0x00020000 unprotected      blank  
Sector 00090: 0xFFB40000 - 0xFFB5FFFF Size=0x00020000 unprotected      blank  
Sector 00091: 0xFFB60000 - 0xFFB7FFFF Size=0x00020000 unprotected      blank  
Sector 00092: 0xFFB80000 - 0xFFB9FFFF Size=0x00020000 unprotected      blank  
Sector 00093: 0xFFBA0000 - 0xFFBBFFFF Size=0x00020000 unprotected      blank  
Sector 00094: 0xFFBC0000 - 0xFFBDFFFF Size=0x00020000 unprotected      blank  
Sector 00095: 0xFFBE0000 - 0xFFBFFFFF Size=0x00020000 unprotected      blank  
Sector 00096: 0xFFC00000 - 0xFFC1FFFF Size=0x00020000 unprotected      blank  
Sector 00097: 0xFFC20000 - 0xFFC3FFFF Size=0x00020000 unprotected      blank  
Sector 00098: 0xFFC40000 - 0xFFC5FFFF Size=0x00020000 unprotected      blank  
Sector 00099: 0xFFC60000 - 0xFFC7FFFF Size=0x00020000 unprotected      blank  
Sector 00100: 0xFFC80000 - 0xFFC9FFFF Size=0x00020000 unprotected      blank  
Sector 00101: 0xFFCA0000 - 0xFFCBFFFF Size=0x00020000 unprotected      blank  
Sector 00102: 0xFFCC0000 - 0xFFCDFFFF Size=0x00020000 unprotected      blank  
Sector 00103: 0xFFCE0000 - 0xFFCFFFFF Size=0x00020000 unprotected      blank  
Sector 00104: 0xFFD00000 - 0xFFD1FFFF Size=0x00020000 unprotected      blank  
Sector 00105: 0xFFD20000 - 0xFFD3FFFF Size=0x00020000 unprotected      blank  
Sector 00106: 0xFFD40000 - 0xFFD5FFFF Size=0x00020000 unprotected      blank  
Sector 00107: 0xFFD60000 - 0xFFD7FFFF Size=0x00020000 unprotected      blank  
Sector 00108: 0xFFD80000 - 0xFFD9FFFF Size=0x00020000 unprotected      blank  
Sector 00109: 0xFFDA0000 - 0xFFDBFFFF Size=0x00020000 unprotected      blank  
Sector 00110: 0xFFDC0000 - 0xFFDDFFFF Size=0x00020000 unprotected      blank  
Sector 00111: 0xFFDE0000 - 0xFFDFFFFF Size=0x00020000 unprotected      blank  
Sector 00112: 0xFFE00000 - 0xFFE1FFFF Size=0x00020000 unprotected      blank  
Sector 00113: 0xFFE20000 - 0xFFE3FFFF Size=0x00020000 unprotected      blank  
Sector 00114: 0xFFE40000 - 0xFFE5FFFF Size=0x00020000 unprotected      blank  
Sector 00115: 0xFFE60000 - 0xFFE7FFFF Size=0x00020000 unprotected      blank  
Sector 00116: 0xFFE80000 - 0xFFE9FFFF Size=0x00020000 unprotected      blank  
Sector 00117: 0xFFEA0000 - 0xFFEBFFFF Size=0x00020000 unprotected      blank  
Sector 00118: 0xFFEC0000 - 0xFFEDFFFF Size=0x00020000 unprotected      blank  
Sector 00119: 0xFFEE0000 - 0xFFEFFFFF Size=0x00020000 unprotected      blank  
Sector 00120: 0xFFF00000 - 0xFFF1FFFF Size=0x00020000 unprotected      blank  
Sector 00121: 0xFFF20000 - 0xFFF3FFFF Size=0x00020000 unprotected      blank  
Sector 00122: 0xFFF40000 - 0xFFF5FFFF Size=0x00020000 unprotected      blank  
Sector 00123: 0xFFF60000 - 0xFFF7FFFF Size=0x00020000 unprotected programmed  
Sector 00124: 0xFFF80000 - 0xFFF9FFFF Size=0x00020000 unprotected programmed  
Sector 00125: 0xFFFA0000 - 0xFFFBFFFF Size=0x00020000 unprotected programmed  
Sector 00126: 0xFFFC0000 - 0xFFFDFFFF Size=0x00020000 unprotected programmed  
Sector 00127: 0xFFFE0000 - 0xFFFFFFFF Size=0x00020000 unprotected programmed  
Flash Information  
=================  
Flash Manufacturer ID     :0x00000001
Flash Device ID (byte1)   :0x0000227E
Flash Device ID (byte2)   :0x00002221
Flash Device ID (byte3)   :0x00002201
Secure Device Verification:0x0000FFBF

I am able to flash VxWorks image using CodeWarrior to these addresses (as you can see above, the memory is "programmed" in the good addresses), but I am not able to execute it, because there is no boot-loader. When I try to reach for this area with U-boot, to copy to memory and initialize, obviously it does not see the area.

If I try to adjust the flash memory map on CodeWarrior, to comply with the documentation (starting at 0xEF000000), CodeWarrior returns an error message that the target flash does not exist / is not available. 

So, I am in a trick situation. I can flash the image and verify it was flashed with codewarrior, but at the same time I have conflicting information with U-boot. The funny part is that Linux images that came with the board were overwritten, but not U-boot. BUT, linux images were also in the 0xEF range, which I supposedly never touched.

Am I missing something here? 

Thanks in advance for the assistance! 

标签 (1)
0 项奖励
回复
1 回复

2,555 次查看
yipingwang
NXP TechSupport
NXP TechSupport

In PowerPC Architecture, memory map is configured by LAW(local access windows), you could refer to "2.4 Local access window registers" in P2020 Reference manual.

In CodeWarrior initialization file 

Freescale\CW_PA_v10.5.1\PA\PA_Support\Initialization_Files\QorIQ_P2\P10xx-P20xxRDB_P2020_init_core.tcl, local bus NOR flash is configured as the following, 0xFF000000 - 0xFFFFFFFF LAW0 is configured for Local Bus NOR FLASH.

# configure local access windows
# LAWBAR0 - Local Bus
# bit 8 - 31 = 0xFF000000 - base addr
mem [CCSR 0xC08] = 0x000ff000

# LAWAR0
# bit 0 = 1 - enable window
# bit 7-11 = 00100 - Local Bus
# bit 26 - 31 = 011011 16M - size
mem [CCSR 0xC10] = 0x80400017

In u-boot, in board/freescale/p1_p2_rdb_pc/law.c, NOR flash is configured as the following.

SET_LAW(CONFIG_SYS_FLASH_BASE_PHYS, LAW_SIZE_64M, LAW_TRGT_IF_LBC),

In include/configs/p1_p2_rdb_pc.h, the macro is definition as the following.

#define CONFIG_SYS_FLASH_BASE_PHYS      CONFIG_SYS_FLASH_BASE

#define CONFIG_SYS_FLASH_BASE           0xef000000

So the memory map in CodeWarrior is different from u-boot.

0 项奖励
回复