Find out CodeWarrior Support Libraries

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Find out CodeWarrior Support Libraries

跳至解决方案
2,779 次查看
vigneshbalaji
Senior Contributor I

Hi,

    How to find out CodeWarrior Support libraries in the CW installed system?

标签 (1)
1 解答
2,628 次查看
trytohelp
NXP Employee
NXP Employee

Hi Vignesh,

You refer to the Start menu and not to the installation folder.

pastedImage_0.png

Regards


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

4 回复数
2,628 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Do you mean C and C++ libs? They are here: C:\Freescale\CW MCU v10.6.4\MCU\ARM_GCC_Support\ewl

Luis

2,628 次查看
vigneshbalaji
Senior Contributor I

Thank you Luis,

                          I am not able to find the file MCU inside CW MCU V10.6.4.I will add screenshots.

Screenshot (20).pngScreenshot (21).png

As you can see in the above picture inside CW MCU V10.6.4 there is no MCU folder

0 项奖励
回复
2,629 次查看
trytohelp
NXP Employee
NXP Employee

Hi Vignesh,

You refer to the Start menu and not to the installation folder.

pastedImage_0.png

Regards


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,628 次查看
vigneshbalaji
Senior Contributor I

Thank you Pascal

0 项奖励
回复