Find out CodeWarrior Support Libraries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Find out CodeWarrior Support Libraries

Jump to solution
2,873 Views
vigneshbalaji
Senior Contributor I

Hi,

    How to find out CodeWarrior Support libraries in the CW installed system?

Labels (1)
1 Solution
2,722 Views
trytohelp
NXP Employee
NXP Employee

Hi Vignesh,

You refer to the Start menu and not to the installation folder.

pastedImage_0.png

Regards


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

4 Replies
2,722 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Do you mean C and C++ libs? They are here: C:\Freescale\CW MCU v10.6.4\MCU\ARM_GCC_Support\ewl

Luis

2,722 Views
vigneshbalaji
Senior Contributor I

Thank you Luis,

                          I am not able to find the file MCU inside CW MCU V10.6.4.I will add screenshots.

Screenshot (20).pngScreenshot (21).png

As you can see in the above picture inside CW MCU V10.6.4 there is no MCU folder

0 Kudos
Reply
2,723 Views
trytohelp
NXP Employee
NXP Employee

Hi Vignesh,

You refer to the Start menu and not to the installation folder.

pastedImage_0.png

Regards


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,722 Views
vigneshbalaji
Senior Contributor I

Thank you Pascal

0 Kudos
Reply