Find out CodeWarrior Support Libraries

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Find out CodeWarrior Support Libraries

ソリューションへジャンプ
2,878件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

    How to find out CodeWarrior Support libraries in the CW installed system?

ラベル(1)
1 解決策
2,727件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Vignesh,

You refer to the Start menu and not to the installation folder.

pastedImage_0.png

Regards


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
2,727件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Do you mean C and C++ libs? They are here: C:\Freescale\CW MCU v10.6.4\MCU\ARM_GCC_Support\ewl

Luis

2,727件の閲覧回数
vigneshbalaji
Senior Contributor I

Thank you Luis,

                          I am not able to find the file MCU inside CW MCU V10.6.4.I will add screenshots.

Screenshot (20).pngScreenshot (21).png

As you can see in the above picture inside CW MCU V10.6.4 there is no MCU folder

0 件の賞賛
返信
2,728件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Vignesh,

You refer to the Start menu and not to the installation folder.

pastedImage_0.png

Regards


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,727件の閲覧回数
vigneshbalaji
Senior Contributor I

Thank you Pascal

0 件の賞賛
返信