Fails to load flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Fails to load flash

跳至解决方案
2,534 次查看
JohnnyP
Contributor III

9S12C32, P&E BDM pod, Metrowerks CW5.5, absolute assembly.

 

It's been working great.  It loads an existing program into the target flash, but will not load the same program when I create a new project and paste the assembly file into the new project.

 

The error says program counter x0000086F operation failed EEPROM flash module.

 

It loads the earlier project just fine.  I created a third project and pasted the file, it fails to load as well.

 

Thanks for any help. 

标签 (1)
0 项奖励
回复
1 解答
2,305 次查看
JohnnyP
Contributor III

Never mind, I accidentally chose 9S12D32.  :smileyhappy:

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,306 次查看
JohnnyP
Contributor III

Never mind, I accidentally chose 9S12D32.  :smileyhappy:

0 项奖励
回复