Fails to load flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Fails to load flash

Jump to solution
2,648 Views
JohnnyP
Contributor III

9S12C32, P&E BDM pod, Metrowerks CW5.5, absolute assembly.

 

It's been working great.  It loads an existing program into the target flash, but will not load the same program when I create a new project and paste the assembly file into the new project.

 

The error says program counter x0000086F operation failed EEPROM flash module.

 

It loads the earlier project just fine.  I created a third project and pasted the file, it fails to load as well.

 

Thanks for any help. 

Labels (1)
0 Kudos
Reply
1 Solution
2,419 Views
JohnnyP
Contributor III

Never mind, I accidentally chose 9S12D32.  :smileyhappy:

View solution in original post

0 Kudos
Reply
1 Reply
2,419 Views
JohnnyP
Contributor III

Never mind, I accidentally chose 9S12D32.  :smileyhappy:

0 Kudos
Reply