Fails to load flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,508件の閲覧回数
JohnnyP
Contributor III

9S12C32, P&E BDM pod, Metrowerks CW5.5, absolute assembly.

 

It's been working great.  It loads an existing program into the target flash, but will not load the same program when I create a new project and paste the assembly file into the new project.

 

The error says program counter x0000086F operation failed EEPROM flash module.

 

It loads the earlier project just fine.  I created a third project and pasted the file, it fails to load as well.

 

Thanks for any help. 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,279件の閲覧回数
JohnnyP
Contributor III

Never mind, I accidentally chose 9S12D32.  :smileyhappy:

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,280件の閲覧回数
JohnnyP
Contributor III

Never mind, I accidentally chose 9S12D32.  :smileyhappy:

0 件の賞賛
返信