FC16

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FC16

1,566 Views
juliancox
Contributor V

I am using a S08QE and Processor Expert. I have a free running counter (FC16 and TPM101) to generate an interrupt every 4ms. With the S08SH everything was fine, as I could set the option to reset on overflow, but I am now using a S08QE and ProcessorExpert tells me that this option is not supported. To get around this problem I have to reset the counter as the first instruction in my ISR. Surely I should not need to do this. 

0 Kudos
Reply
1 Reply

1,448 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Julian Cox,

"tells me that this option is not supported. ", could you please take a screenshot tell us which option ,

does it in the Processor  Expert component configuration ?

BR

Alice

0 Kudos
Reply