FC16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FC16

1,593件の閲覧回数
juliancox
Contributor V

I am using a S08QE and Processor Expert. I have a free running counter (FC16 and TPM101) to generate an interrupt every 4ms. With the S08SH everything was fine, as I could set the option to reset on overflow, but I am now using a S08QE and ProcessorExpert tells me that this option is not supported. To get around this problem I have to reset the counter as the first instruction in my ISR. Surely I should not need to do this. 

0 件の賞賛
返信
1 返信

1,475件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Julian Cox,

"tells me that this option is not supported. ", could you please take a screenshot tell us which option ,

does it in the Processor  Expert component configuration ?

BR

Alice

0 件の賞賛
返信