Error: Hi wave Parameter File Could Not Be Loaded

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error: Hi wave Parameter File Could Not Be Loaded

ソリューションへジャンプ
2,180件の閲覧回数
tnriley
Contributor III

I installed the Code Warrior 5.2 Missing pieces files and everything seems to work ok except for an issue with a parameter file for a H-Wave debugger.

 

Error Message: "Hi wave Parameter File Could Not Be Loaded" I don't use this debugger so it should not be an issue, but are there any updates for those that might.

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,926件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Tim

What chip do you working with?

One possible reason is that your CW project didn't use correct fpp file.

Different chip uses different algorithm file (*.fpp). You can check it in debugger menu "H12MultilikCyclonePro", "Flash"

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,927件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Tim

What chip do you working with?

One possible reason is that your CW project didn't use correct fpp file.

Different chip uses different algorithm file (*.fpp). You can check it in debugger menu "H12MultilikCyclonePro", "Flash"

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------