Error: Hi wave Parameter File Could Not Be Loaded

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error: Hi wave Parameter File Could Not Be Loaded

Jump to solution
2,229 Views
tnriley
Contributor III

I installed the Code Warrior 5.2 Missing pieces files and everything seems to work ok except for an issue with a parameter file for a H-Wave debugger.

 

Error Message: "Hi wave Parameter File Could Not Be Loaded" I don't use this debugger so it should not be an issue, but are there any updates for those that might.

 

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
1,975 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Tim

What chip do you working with?

One possible reason is that your CW project didn't use correct fpp file.

Different chip uses different algorithm file (*.fpp). You can check it in debugger menu "H12MultilikCyclonePro", "Flash"

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,976 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Tim

What chip do you working with?

One possible reason is that your CW project didn't use correct fpp file.

Different chip uses different algorithm file (*.fpp). You can check it in debugger menu "H12MultilikCyclonePro", "Flash"

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------