Error: Hi wave Parameter File Could Not Be Loaded

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error: Hi wave Parameter File Could Not Be Loaded

跳至解决方案
2,209 次查看
tnriley
Contributor III

I installed the Code Warrior 5.2 Missing pieces files and everything seems to work ok except for an issue with a parameter file for a H-Wave debugger.

 

Error Message: "Hi wave Parameter File Could Not Be Loaded" I don't use this debugger so it should not be an issue, but are there any updates for those that might.

 

Thanks

标签 (1)
0 项奖励
回复
1 解答
1,955 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Tim

What chip do you working with?

One possible reason is that your CW project didn't use correct fpp file.

Different chip uses different algorithm file (*.fpp). You can check it in debugger menu "H12MultilikCyclonePro", "Flash"

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,956 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Tim

What chip do you working with?

One possible reason is that your CW project didn't use correct fpp file.

Different chip uses different algorithm file (*.fpp). You can check it in debugger menu "H12MultilikCyclonePro", "Flash"

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------