Dragon12-Plus2 MC9S12DG256

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dragon12-Plus2 MC9S12DG256

ソリューションへジャンプ
3,691件の閲覧回数
davidstaheli
Contributor I

I downloaded the special edition Codewarrior V5.2 and saw that it does not support my micro-controller. I saw that the 5.1 version does but is only available for evaluation. Are any there downloads available that will allow me to use my controller in V5.2, or is the old version available anywhere. I am not going to spend a lot of money to get it. I'm a student and just using it for one semester for an embedded systems class. Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,251件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi David,

the difference between CW5.1 special edition and evaluation edition is license.dat file.

CW5.1 special edition uses special edition license.dat

CW5.1 evaluation edition uses evaluation edition license.dat.

so if you want to use CW5.1 special edition, you can install CW5.1 evaluation edition from

CodeWarrior Legacy Downloads|NXP

the replace {your CW5.1 install}\license.dat with attached special edition license.dat

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,251件の閲覧回数
davidstaheli
Contributor I

Thanks to everyone for the replies. Your suggestions were very helpful.

0 件の賞賛
返信
3,251件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello David

Please refer to the link below for how to download CW5.1 for HCS12:

https://community.freescale.com/thread/382638

Hope this helps!

Best Regards

Fiona Kuang

Technical Information & Commercial Support

0 件の賞賛
返信
3,251件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi David,

In addition to Jennie ...

We've an University Program too.

Don't know if this could be interesting for you:

    University Programs|NXP


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,252件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi David,

the difference between CW5.1 special edition and evaluation edition is license.dat file.

CW5.1 special edition uses special edition license.dat

CW5.1 evaluation edition uses evaluation edition license.dat.

so if you want to use CW5.1 special edition, you can install CW5.1 evaluation edition from

CodeWarrior Legacy Downloads|NXP

the replace {your CW5.1 install}\license.dat with attached special edition license.dat

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信