Does Codewarrior V10.6.4 support MKL17Z64 series? I can't find this part in CW10.6.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does Codewarrior V10.6.4 support MKL17Z64 series? I can't find this part in CW10.6.4

790件の閲覧回数
huaping
Contributor III

does Codewarrior V10.6.4 support MKL17Z64 series? I can't find this part number in CW10.6.4.

is there any package to support?

Thanks!

ラベル(1)
0 件の賞賛
返信
1 返信

625件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

CW v10.6.4 doesn't support MKL17Z64 series. CW is in maintenance mode, so there is no plan to add new device to it.

NXP KDS can support MKL17Z64 series:

www.nxp.com/kds

does this answer your question?
Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信