Does codewarrior10.6.4 can use command line tools to download s19 or mot file to MPC5604B?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does codewarrior10.6.4 can use command line tools to download s19 or mot file to MPC5604B?

1,288 Views
maoyuanluo
Contributor III

Does codewarrior10.6.4 can use command line tools to download s19 or mot file to MPC5604B?

Labels (1)
0 Kudos
Reply
3 Replies

1,138 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

there is a debugger directly included in CodeWarrior IDE, which also supports Debugger shell. This debugger can download elf files and also mot files or s19 files into microcontroller.

There is no independent command line tools (neither independent application) which can be executed without CodeWarrior IDE. This is supported in S32 Design Studio where GDB server and GDB client is used.

Regards,

Martin

1,138 Views
maoyuanluo
Contributor III

can you provide the Operation manual for s32 design studio which use command line tools to download debug file?

0 Kudos
Reply

1,138 Views
maoyuanluo
Contributor III

Thank you for your answer!

0 Kudos
Reply