Does codewarrior10.6.4 can use command line tools to download s19 or mot file to MPC5604B?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does codewarrior10.6.4 can use command line tools to download s19 or mot file to MPC5604B?

1,307 次查看
maoyuanluo
Contributor III

Does codewarrior10.6.4 can use command line tools to download s19 or mot file to MPC5604B?

标签 (1)
0 项奖励
回复
3 回复数

1,157 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

there is a debugger directly included in CodeWarrior IDE, which also supports Debugger shell. This debugger can download elf files and also mot files or s19 files into microcontroller.

There is no independent command line tools (neither independent application) which can be executed without CodeWarrior IDE. This is supported in S32 Design Studio where GDB server and GDB client is used.

Regards,

Martin

1,157 次查看
maoyuanluo
Contributor III

can you provide the Operation manual for s32 design studio which use command line tools to download debug file?

0 项奖励
回复

1,157 次查看
maoyuanluo
Contributor III

Thank you for your answer!

0 项奖励
回复