Device EA series not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Device EA series not found

3,834 Views
ddpd
Contributor III

Just received the TRK KEA 128 kinetis board. I downloaded the code warrior. But while creating a new project the series EA is not found.

There is only K, L, M and N series available. Do you recommend to use the same IDE or any other IDE's for this development board.

Labels (1)
0 Kudos
Reply
3 Replies

3,592 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Dino

KEA128 is supported from CodeWarrior v10.6. The attached is its release note.

The latest version is v10.6.5.

Please first install CW10.6.4 which can be downloaded from:

www.freescale.com/cwmcu10

Its update v10.6.5 is also available at the same link.

Further information and the release notes are available on the following Freescale community page:

https://community.freescale.com/docs/DOC-143655

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,592 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Dino,

please which version CW are you using?

You always choose what you want to install during the installation.

CW_.png

There is support for MCU KEA128

On my side, CW 10.6

CW.png

I hope this helps.

Best Regards,

Iva

0 Kudos
Reply

3,592 Views
ddpd
Contributor III

My codewarrior version was 10.5. I will update the version.

Thanks for the reply

0 Kudos
Reply