Debug MC9S12XDP512 with HiWave 6.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug MC9S12XDP512 with HiWave 6.1

2,029 Views
christianfrick
Contributor I

We are trying to debug a MC9S12XDP512VAL processor with HiWave 6.1 but it seems like it is not supported anymore (with former versions it was).

I'm wondering if there is any Windows 7 capable tool which is still capable to debug a MC9S12XDP512VAL processor?

0 Kudos
Reply
3 Replies

1,820 Views
gredolfo
Contributor I

Could you please post an updated procedure or a link to download CodeWarrior v5.1. We are having the same problem with CodeWarrior v5.2 and MC9S12DB128B. Also, CodeWarrior v5.1 is not compatible with Windows 10 64 bit. We need Hiwave to load to the microcontroller and Hiwave from CodeWarrior v5.2 is missing its derivative.

Thanks

0 Kudos
Reply

1,820 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Gary.

This post is from one year ago. we won't maintain it anymore.

Please create a new thread for your questions, we will be ready for help.

Best Regards

Jennie Zhang

0 Kudos
Reply

1,820 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Christian.

CW 5.2 can only support limited device.
 This release includes support for the following derivatives:
 - MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96
 - MC9S12G128, MC9S12G96
 - MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64
 - MC9S12GN16, MC9S12GN32
 - MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128
 - MC9S12XEP100, MC9S12XEP768
 - MC9S12XEQ384, MC9S12XEQ512
 - MC9S12XET256
 - MC9S12XS128, MC9S12XS256, MC9S12XS64
 - MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64
 
 user who needs to work with other HCS12(x) device, please use CW5.1. I attached a
 video for how to download CW5.1.

CW5.1 supports this platform:

  • Microsoft® Windows® XP 32-bit and 64-bit
  • (Professional Edition)
  • Microsoft Windows Vista® Business 32-bit
  • Microsoft Windows Vista Home Premium 32-bit
  • Microsoft Windows Vista Business 64-bit
  • Microsoft Windows 7 32-bit and 64-bit (Home
  • Premium and Professional Edition)


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply