DDR validition D_INIT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR validition D_INIT

2,170 Views
matthewboutin
Contributor I

P1011 DDR3 clock centering validation fails with D_INIT. Some cells pass, some fail. We turn EEC on and we get more failures. Should we leave ECC off to run this test. Also READ ODT and WRITE ODT all fail with D_INIT when we use the WRLVL and CLK adjust settings when ECC was on. If we use the clock centering values we obtained with ECC off READ ODT and WRITE ODT passes some values. Signal integrity looks good.

0 Kudos
Reply
2 Replies

1,861 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Matthew Boutin,

Please check DDR controller configuration in CW initialization file, whether these two bits DDR_SDRAM_CFG[ECC_ON]  and DDR_SDRAM_CFG_2[D_INIT]  are set when ECC is on.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,861 Views
matthewboutin
Contributor I

Hello Yiping,

Thank You for the reply. The settings above were correct during our testing. We found that DDR_Reset was not toggling when the JTAG POD HRESET was toggling which gave us bad results. This is an undocumented requirement for the tool. After connecting HRESET to DDR_Reset our results were good.  It would be good to have this requirement documented in an application note or specification for the memory validation tool.

Thank You for your reply

mb

0 Kudos
Reply